You are here: TI-Basic Programming Guide for the TI CE Family of Graphing Calculators > Creating and Deleting Programs > Creating a New Program

Creating a New Program

To create a new program, follow these steps.

1. Press ¼ | to display the PRGM NEW menu.

2. Press Í to select 1:Create New. The Name= prompt is displayed, and alpha-lock is on.
3. Press a letter from A to Z or q to enter the first character of the new program name.

Note: A program name can be one to eight characters long. The first character must be a letter from A to Z or q. The second through eighth characters can be letters, numbers, or q.

4. Enter zero to seven letters, numbers, or q to complete the new program name.
5. Press Í. The program editor is displayed.
6. Enter one or more program commands.
7. Press y 5 to leave the program editor and return to the home screen.