|
Error Message |
Description |
|---|---|
|
Arithmetic Error |
This is a general error caused by a limitation error (such as an overflow error when a result is ≥ 1E100) or a mathematical error (such as divide-by-zero). |
|
Err: Memory |
This error occurs when the graphing calculator does not have enough free RAM to perform the operation. Also, if the unit has less than XXXX bytes, the application will not start. |
|
Fit Error |
This error occurs when a regression fit cannot be performed on a scatterplot or xyline plot, because the data in the lists is not compatible with that type of regression. The error also occurs if you press É to break (stop) a regression fit calculation in progress. |
|
Input Error |
This error occurs when an invalid entry is entered into an editor field. For example, an error occurs if you enter 1..2 instead of 1.2. |
|
Stat Error |
This error occurs if you select STAT to perform a one-variable statistical calculation on a list containing data that is incompatible with one-variable analysis. |
See the graphing calculator’s Reference Guide for information on system error messages.
See the original app guidebook for more details on this application. Visit education.ti.com/go/download.