|
|
|
|---|---|
|
ZBox Displays a graph, lets you draw a box that defines a new viewing window, and updates the window. |
† q |
|
|
|
|---|---|
|
ZDecimal Adjusts the viewing window so that TraceStep=0.1, @X=0.5 and @Y=0.5, and displays the graph screen with the origin centred on the screen. |
† q |
|
ZFrac1/2 |
|
|---|---|
|
ZFrac1/2 Sets the window variables so that you can trace in increments of |
q |
|
ZFrac1/3 |
|
|---|---|
|
ZFrac1/3 Sets the window variables so that you can trace in increments of |
q |
|
ZFrac1/4 |
|
|---|---|
|
ZFrac1/4 Sets the window variables so that you can trace in increments of |
q |
|
ZFrac1/5 |
|
|---|---|
|
ZFrac1/5 Sets the window variables so that you can trace in increments of |
q |
|
ZFrac1/8 |
|
|---|---|
|
ZFrac1/8 Sets the window variables so that you can trace in increments of |
q |
|
ZFrac1/10 |
|
|---|---|
|
ZFrac1/10 Sets the window variables so that you can trace in increments of |
q |
|
|
|
|---|---|
|
ZInteger Redefines the viewing window using the following dimensions: TraceStep=1, @X=0.5, Xscl=10, @Y=1, Yscl=10. |
† q |
|
|
|
|---|---|
|
ZIntervals[,listname,freqlist,confidence level] Computes a z confidence interval. |
† … |
|
ZInterval |
|
|---|---|
|
ZIntervals,v,n[,confidence level] Computes a z confidence interval. |
† … |
|
|
|
|---|---|
|
Zoom In Magnifies the part of the graph that surrounds the cursor location. |
† q |
|
|
|
|---|---|
|
Zoom Out Displays a greater portion of the graph, centred on the cursor location. |
† q |
|
|
|
|---|---|
|
ZoomFit Recalculates Ymin and Ymax to include the minimum and maximum Y values, between Xmin and Xmax, of the selected functions and replots the functions. |
† q |
|
|
|
|---|---|
|
ZoomRcl Graphs the selected functions in a user-defined viewing window. |
† q |
|
|
|
|---|---|
|
ZoomStat Redefines the viewing window so that all statistical data points are displayed. |
† q |
|
|
|
|---|---|
|
ZoomSto Immediately stores the current viewing window. |
† q |
|
|
|
|---|---|
|
ZPrevious Replots the graph using the window variables of the graph that was displayed before you executed the last ZOOM instruction. |
† q |
|
ZQuadrant1 |
|
|---|---|
|
ZQuadrant1 Displays the portion of the graph that is in quadrant 1. |
q |
|
|
|
|---|---|
|
ZSquare Adjusts the X or Y window settings so that each pixel represents an equal width and height in the coordinate system, and updates the viewing window. |
† q |
|
|
|
|---|---|
|
ZStandard Replots the functions immediately, updating the window variables to the default values. |
† q |
|
|
|
|---|---|
|
Z‑Test(m0,s[,listname,freqlist,alternative,drawflag,colour#]) Performs a z test with frequency freqlist. alternative= L1 is <; alternative=0 is ; alternative=1 is >. drawflag=1 draws results; drawflag=0 calculates results. Colour#: 10 - 24 or colour name pasted from [vars] COLOUR. |
† … |
|
Z‑Test( |
|
|---|---|
|
Z‑Test(m0,s,v,n[,alternative,drawflag,colour#]) Performs a z test. alternative=L1 is <; alternative=0 is ; alternative=1 is >. drawflag=1 draws results; drawflag=0 calculates results. Colour#: 10 - 24 or colour name pasted from [vars] COLOUR. |
† … |
|
|
|
|---|---|
|
ZTrig Replots the functions immediately, updating the window variables to preset values for plotting trig functions. |
† q |