|
|
|
|---|---|
|
GarbageCollect Displays the garbage collection menu to allow cleanup of unused archive memory. |
y N |
|
|
|
|---|---|
|
gcd(valueA,valueB) Returns the greatest common divisor of valueA and valueB, which can be real numbers or lists. |
» |
|
|
|
|---|---|
|
geometcdf(p,x) Computes a cumulative probability at x, the number of the trial on which the first success occurs, for the discrete geometric distribution with the specified probability of success p. |
y = |
|
|
|
|---|---|
|
geometpdf(p,x) Computes a probability at x, the number of the trial on which the first success occurs, for the discrete geometric distribution with the specified probability of success p. |
y =
|
|
|
|
|---|---|
|
Get(variable) Retrieves a value from a connected TI-Innovator™ Hub and stores the data to a variable on the receiving CE calculator. |
† ¼ |
|
Ti-Innovator™ Hub |
|
|---|---|
|
Get(variable) Retrieves a value from a connected TI-Innovator™ Hub and stores the data to a variable on the receiving CE calculator. |
† ¼ |
|
|
|
|---|---|
|
GetCalc(variable[,portflag]) Gets contents of variable on another TI‑84 Plus CE and stores it to variable on the receiving TI‑84 Plus CE. By default, the TI‑84 Plus CE uses the USB port if it is connected. If the USB cable is not connected, it uses the I/O port. |
† ¼ |
|
|
|
|---|---|
|
getDate Returns a list giving the date according to the current value of the clock. The list is in {year,month,day} format. |
y N |
|
|
|
|---|---|
|
getDtFmt Returns an integer representing the date format that is currently set on the device. 1 = M/D/Y |
y N |
|
|
|
|---|---|
|
getDtStr(integer) Returns a string of the current date in the format specified by integer, where: 1 = M/D/Y |
y N |
|
|
|
|---|---|
|
getTime Returns a list giving the time according to the current value of the clock. The list is in {hour,minute,second} format. The time is returned in the 24 hour format. |
y N |
|
|
|
|---|---|
|
getTmFmt Returns an integer representing the clock time format that is currently set on the device. 12 = 12 hour format |
y N |
|
|
|
|---|---|
|
getTmStr(integer) Returns a string of the current clock time in the format specified by integer, where: 12 = 12 hour format |
y N |
|
|
|
|---|---|
|
getKey Returns the key code for the current keystroke, or 0, if no key is pressed. |
† ¼ |
|
|
|
|---|---|
|
Gotolabel Transfers control to label. |
† ¼ |
|
|
|
|---|---|
|
GraphColour(function#,colour#) Sets the colour for function#. Colour#: 10 - 24 or colour name pasted from [vars] COLOUR. |
† ¼ |
|
|
|
|---|---|
|
GraphStyle(function#,graphstyle#) Sets a graphstyle for function#. |
† ¼ |
|
|
|
|---|---|
|
GridDot [colour#] Turns on grid dots in the graph area in the specified colour. Colour#: 10 - 24 or colour name pasted from [vars] COLOUR. |
† y . |
|
|
|
|---|---|
|
Turns on grid lines in the graph area in the specified colour. Colour#: 10 - 24 or colour name pasted from [vars] COLOUR. |
† y . |
|
|
|
|---|---|
|
GridOff Turns off grid format. |
† y . |
|
G-T |
|
|---|---|
|
G-T Sets graph-table vertical split-screen mode. |
† z |