The TI-84 Plus CE graphing calculator has many color options and a high resolution display that allows more information to be shown on the screen. The TI-84 Plus CE uses color in the following ways:
•
Y= editor for line color.
•
DRAW commands for line color, such as vertical lines, circles, and text on the graph screen.
•
The graph format screen for grid, axes, or border color, and applying a background image or color.
•
Statistical Plots.
Color options for various features are accessed via a spinner menu. With the cursor on a color selection for a feature, use the | or ~ to change the color. When the cursor is on any spinner menu, the context help in the status bar frequently displays the hint: PRESS [<] OR [>] TO SELECT AN OPTION.
Note: Take care to choose appropriate color combinations for the graph areas so that all features are visible.
Resetting Color Options to Default
•
With the cursor on a function in [Y=], press ‘‘ to return to the default color and line style for that function.
•
You can reset the calculator to its default settings, including color settings, by pressing yL7 2 2.