Note: TI Connect™ CE software is available as a free download from education.ti.com/go/download.
• | Pic Vars (Pic1 - Pic 9, and Pic0) are also variables stored in archive memory. Pic Vars can be created by drawing in the graphing area, and the changes saved and recalled to the graphing area. Saving a Pic Var will not include the Background Image behind your graphing area. |
• | Both Image Vars and Pic Vars are stored and run in Flash archive, not in RAM. They are both accessible in the VARS menu. |
• | Image Vars and Pic Vars can only be shared with another TI-84 Plus CE or TI-84 C graphing calculator. |
• | TI-84 Plus Pic Vars cannot be shared between the TI-84 Plus and the TI-84 Plus CE graphing calculators. |
• | If you perform a RAM reset on the TI-84 Plus CE , the Image Vars and Pic Vars remain in Archive memory for use. |