The following rules are applied when using the Transformation Graphing App:
| • | Allows Y1 and/or Y2 to transform using parameters A, B, C, or D in the functions. Graphing using Y3-Y0 is allowed, however, A-D, Y1 and Y2 are not allowed in Y3-Y0. |
| • | p setting Xres=3 is set for animations. Set Xres=1 in [window] for default graphing if needed when only graphing in Y3-Y0. |
| • | Up to three stat plots can be graphed. |
| • | Recommend using QUIT-APP in [Y=] when not transforming graphs. |
If any of these rules are broken, the following message will appear and the offending Y-Vars are disabled and the remaining graphs will appear.