Use this activity to learn the basics the Transformation Graphing App.
Note: Reset the calculator defaults (y L 7:Reset..., 2:Defaults..., 2:Reset) before this performing this activity.
|
|
|||||||||||||||
Note: The color/line style spinner dialog also lets you select the animation of the transform graph. Play-Pause 3 will allow you to control the animation of the graph using the arrow keys on the graph screen. |
|
|||||||||||||||
|
Tip: If you enter a function using the keypad, only A-D are allowed in transform equations Y1 and/or Y2. Those letters can be found using the ƒ key. For example, to enter the coefficient A, press ƒ [A] (above the » key).
|
||||||||||||||||
|
|
|||||||||||||||
If the coefficient A is not selected, press † until the = sign for A is highlighted. |
|
|||||||||||||||
|
|
|||||||||||||||
|
Tip: Press [SETUP] (b) on the graph screen to display the SETTINGS menu. Select TrailOn to leave a dotted graph each time you change or animate a coefficient. Default is TrailOff. TrailOff and TrailOn are also available in y .. The play 1 and play fast 2 settings allow you to create animated slide show of the graph transforming by one selected parameter. The parameter values for A-D can be entered in SETTINGS as long as they are used in Y1 and/or Y2. The Step value determines the increment of the parameter value. The Max value is the upper bound of the parameter expected in the animation. Example: Y1=AX In SETTINGS, let A=1, Step = 2, and Max = 10. Five screens will be created to animate the graph for A = 1, 3, 5, 7, 9. Note 9 < 10 = Max. There can be up to 13 screens created for the animation. A memory error will be given if the Step and Max request more than 13 screens for the animation. To continue, press p and press } to SETTINGS. Modify the Step or Max value to remain within the 13 screen limit. |
|
|||||||||||||||
Note: Enter a quadratic function in vertex form to graph in Y3. Try to match Y1 to the graph of Y3!