To quit the App, press [Quit] (s).
|
Menus |
Functions |
|---|---|
|
Main Menu |
|
|
File |
Save the data from an experiment or select New and Vernier EasyData™ App restarts in the default data-collection mode, and the default settings are restored. |
|
Setup |
Set up the experiment. The menu will differ depending on the sensor. For example, for connected CBR 2™ motion detector, the setup menu displays as follows:
|
|
Time Graph |
Open the Time Graph Settings wizard. |
|
Sample Interval |
Set the interval in seconds. Select Next to go to the next setting. |
|
Number of Samples |
Set the total number of samples to collect. |
|
Experiment Length |
Set the length of the experiment in seconds. |
|
Edit |
Edit the time graph settings. |
|
Cancl |
Cancel your changes and return to the previous settings. |
|
OK |
Return to the main menu. |
|
Events with Entry |
Capture samples manually for a set of events that you define. Each sampled value becomes a y-value; you enter the x-value. |
|
Keep |
Capture the current sampled (y) value. |
|
Enter value |
Assign an x-value to define the data point. Then select OK. |
|
Stop |
Select Stop to end the experiment. The data points are displayed as a graph (a calculator scatter plot). |
|
Main |
Return to the main menu. |
|
Zero |
Use the current data reading as a zero reference. |
|
Start |
Start collecting data. |
|
Stop |
Stop collecting data. A scaled graph of the collected data appears. |
|
Main |
Return to the main menu. |
|
Graph |
Graph the resulting equation. |
|
Adv |
Select independent and dependent lists to plot various views of the data. |
|
Plots |
Plot options such as distance vs. time, velocity vs. time, and acceleration vs. time (dependent on sensor connected). |
|
Anlyz |
Computes statistics on data collected and finds a variety of regression fit to data (dependent on sensor connected). |
|
Scale |
Options to auto-fit or manually edit the graph scaling. |
|
Quit |
Quit the application. The collected data has been transferred to the calculator’s lists. |