Copying and Renaming a Program
To copy all command lines from one program into a new program, follow steps 1 through 4 for Creating a New Program, and then follow these steps.
|
1.
|
Press y K. Rcl is displayed on the bottom line of the program editor in the new program. |
|
2.
|
Press ¼ to display the menu. |
|
3.
|
Select a name from the menu. prgmname is pasted to the bottom line of the program editor. |
|
4.
|
Press Í. All command lines from the selected program are copied into the new program. |
Copying programs has at least two convenient applications.
|
•
|
You can create a template for groups of instructions that you use frequently. |
|
•
|
You can rename a program by copying its contents into a new program. |
Note: You also can copy all the command lines from one existing program to another existing program using RCL.