Browsing the TI-84 Plus CE-T Catalogue Help

Selecting an Item from the CATALOGUE

To browse and select a CATALOGUE item, follow these steps.

1. Press y Nto display the CATALOGUE.

The 4 in the first column is the selection cursor.

2. Press or } to scroll the CATALOGUE until the selection cursor points to the item you want.
To jump to the first item beginning with a particular letter, press that letter; alpha-lock is on.
Items that begin with a number are in alphabetical order according to the first letter after the number. For example, 2‑PropZTest( is among the items that begin with the letter P.
Functions that appear as symbols, such as +, L1, <, and $(, follow the last item that begins with Z. To jump to the first symbol, !, press [q].
3. Press Í to paste the item to the current screen.

Note:

From the top of the CATALOGUE menu, press } to move to the bottom. From the bottom, press to move to the top.
When your TI‑84 Plus CE-T is in MathPrint™ mode, many functions will paste the MathPrint™ template on the home screen. For example, abs( pastes the absolute value template on the home screen instead of abs(.


MathPrint™


Classic