RV.GRID.ORIGIN

Command:

RV.GRID.ORIGIN

Command Syntax:

RV.GRID.ORIGIN

Code
Sample:

Send "SET RV.GRID.ORIGIN"

 

[SET} RV.GRID.ORIGIN

Range:

N/A

Describe:

Sets RV as being at current grid origin point of (0,0). The "heading" is set to 0.0 resulting in the current position of the RV now set to pointing down a virtual x-axis toward positive x values.

Result:

 

Type or
Addressable Component:

Setting