|
Command: |
RV.RANGER |
||||
|---|---|---|---|---|---|
|
Command Syntax: |
RV.RANGER |
||||
|
Code |
Send("READ RV.RANGER") Get(R)
|
||||
|
Range: |
N/A |
||||
|
Describe: |
The front-facing ultrasonic distance sensor. Returns measurements in meters. ~10.00 meters means no obstacle was detected.
|
||||
|
Result: |
Returns value in Meters. |
||||
|
Type or |
Sensor Note: This Rover sensor command is executed immediately. |
|
Command: |
READ RV.RANGER TIME |
|---|---|
|
Command |
READ RV.RANGER TIME |
|
Range: |
|
|
Describe: |
Additional functionality for RV.RANGER - to return time of flight instead of distance. The value is in seconds. And it is the round trip time for the signal. |
|
Result: |
Retrieves the time-of-flight data readings for the RANGER on TI-Innovator™ Rover. |
|
Type or |
Sensor |