|
Command: |
CONNECT RGB |
|---|---|
|
Command Syntax: |
CONNECT RGB |
|
Code |
Send "CONNECT RGB" |
|
Range: |
N/A |
|
Describe: |
The "CONNECT RGB" command configures the TI-Innovator™ Hub software to work with the TI-RGB Array. |
|
Result: |
Connects the TI-RGB Array to the TI-Innovator™ Hub. The TI-RGB Array is now ready to be programmed |
|
Type or |
All components of the TI-RGB Array. See Also: Commands to use with TI-RGB Array |
|
Command: |
CONNECT RGB AS LAMP |
|---|---|
|
Command Syntax: |
CONNECT RGB AS LAMP |
|
Code |
Send "CONNECT RGB AS LAMP" |
|
Range: |
N/A |
|
Describe: |
This command will enable the “high brightness” mode of the TI-RGB Array as long as an external power source (like the USB battery) is connected to the PWR port. Note: “AS LAMP” will need to be typed in. |
|
Result: |
The TI-RGB Array is now configured to be in high-brightness mode. If the external power is not connected, the “AS LAMP” has no effect – i.e. the brightness will be at the default level. Also note, an error will be indicated by a beep tone. |
|
Type or |
All components of the TI-RGB Array. See Also: Commands to use with TI-RGB Array |