Normally, the TI‑Innovator™ Hub and its connected components draw power from the host calculator or computer, through the DATA connector. Certain components, such as the optional Servo Motor, require more power than a calculator can provide reliably.
The PWR connector on the Hub lets you connect an auxiliary power source. You can use the TI Wall Charger or the External Battery Pack.
TI Wall Charger (included with the
|
|
|||||||||
External Battery Pack (sold separately)
Note: To recharge the External Battery Pack, disconnect it from the Hub and then connect it to the TI Wall Charger using the USB Standard A to Micro cable. Do not use the External Battery Pack as an auxiliary power source while it is being charged. |
![]() |
|
|
3. | Insert the free end of the cable (the "A" connector) into the USB port on the power source. |
4. | Turn on the power source: |
- | If using the TI Wall Charger, plug it into a wall socket. |
- | If using the External Battery Pack, press the power button. |
An auxiliary power LED on the
5. | Connect the TI‑Innovator™ Hub to the host calculator, using the USB Standard A to Mini‑B cable. |
6. | Connect the I/O Module or breadboard component to the |