FORMAT ERROR STRING/NUMBER

Command:

FORMAT ERROR STRING/NUMBER

Advanced user

Command Syntax:

SET FORMAT ERROR STRING/NUMBER

Range:

 

Describe:

Used for setting error return format and optional audible tone on error.

SET FORMAT ERROR STRING/NUMBER – returned error codes in string or numeric format.

Result:

Sets the format for the return of error information (numbers, or strings).

Type or
Addressable Component:

Setting

 

FORMAT ERROR NOTE/QUIET

Command:

FORMAT ERROR NOTE/QUIET

Advanced user

Command Syntax:

SET FORMAT ERROR NOTE/QUIET

Range:

 

Describe:

Used for setting error return format and optional audible tone on error.

SET FORMAT ERROR NOTE/QUIET – error display flash accompanied by speaker sound or no sound.

Result:

Enables tones, or disables tones in addition to the string/number reporting above.

Type or
Addressable Component:

Setting