Command: |
TEMPERATURE i
|
---|---|
Command Syntax: |
READ TEMPERATURE i |
Range: |
Temperature reading default is in Celsius. The range depends on the specific temperature sensor being used. Humidity reading from 0 to 100 % |
Describe: |
Returns the current temperature reading from the associated temperature sensor. The temperature is given, by default, in Celsius. READ TEMPERATURE i |
Result: |
Return current temperature reading in Celsius. |
Type or |
Sensor |
Command: |
TEMPERATURE i AVERAGE Advanced user
|
---|---|
Command Syntax: |
READ TEMPERATURE i AVERAGE |
Range: |
Temperature reading default is in Celsius. The range depends on the specific temperature sensor being used. Humidity reading from 0 to 100 % |
Describe: |
Returns the current temperature reading from the associated temperature sensor. The temperature is given, by default, in Celsius. READ TEMPERATURE i AVERAGE |
Result: |
Return current temperature reading in Celsius. |
Type or |
Sensor |
Command: |
TEMPERATURE i CALIBRATION
Advanced user
|
---|---|
Command Syntax: |
READ TEMPERATURE i CALIBRATION |
Range: |
Temperature reading default is in Celsius. The range depends on the specific temperature sensor being used. Humidity reading from 0 to 100 % |
Describe: |
Returns the current temperature reading from the associated temperature sensor. The temperature is given, by default, in Celsius. |
Result: |
Returns list with current {c1,c2,c3,r} values used for connected analog temperature sensor. |
Type or |
Sensor |