PWR

Command:

PWR

Command Syntax:

READ PWR

Range:

 

Describe:

Returns the current state of presence of external power connected to the PWR port. The PWR port is read, and a status value of 0 (not present) or 1 (present) is returned, based on whether or not external power is available.

READ PWR

Result:

Returns state of external power presence on PWR port (0=not present, 1=ext pwr present).

Type or
Addressable Component:

Status