MOTION i

Command:

MOTION i

 

Command Syntax:

READ MOTION i

Range:

 

Describe:

Return the current PIR Motion sensor information. PIR Motion sensors are digital in nature, so are treated similar to a button in that the value returned indicates motion presence or not.

0=no motion detected.

1=motion detected.

2=motion was detected.

Result:

Read state of PIR Motion detector - 0=no motion, 1=motion, 2=motion was detected but none now.

Type or
Addressable Component:

Sensor