Command: |
MOISTURE i
|
---|---|
Command Syntax: |
READ MOISTURE i |
Range: |
An integer value between 0 and 16383 (14 bit resolution) |
Describe: |
Return the current analog level reported by the moisture sensor specified. Supports the AVERAGE and RANGE options. READ MOISTURE i READ MOISTURE i AVERAGE READ MOISTURE i RANGE |
Result: |
Read analog value of moisture sensor (uses averaging). |
Type or |
Sensor |
Command: |
MOISTURE i AVERAGE Advanced user
|
---|---|
Command Syntax: |
READ MOISTURE i AVERAGE |
Range: |
|
Describe: |
Return the current analog level reported by the moisture sensor specified. Supports the AVERAGE and RANGE options. READ MOISTURE i AVERAGE |
Result: |
Read analog value of moisture sensor (uses averaging). |
Type or |
Sensor |
Command: |
MOISTURE i RANGE
|
---|---|
Command Syntax: |
READ MOISTURE i RANGE |
Range: |
|
Describe: |
Return the current analog level reported by the moisture sensor specified. Supports the AVERAGE and RANGE options. READ MOISTURE i RANGE |
Result: |
Read analog value of moisture sensor (uses averaging). |
Type or |
Sensor |