Command: |
FORMAT
Advanced user
|
---|---|
Command Syntax: |
READ FORMAT |
Range: |
|
Describe: |
Return the current formatting flags for error reporting. The value returned is a byte value indicating various flags. Masking with values indicates what error reporting options are active. 1 = ERROR strings reported 2 = ERROR numbers reported +4 = ERROR TONE enabled, if not set, errors are reported silently. |
Result: |
Read error format (1=strings, 2=numbers, +4 to either: tones enabled). |
Type or |
Setting |