Command: |
BRIGHTNESS
|
---|---|
Command Syntax: |
READ BRIGHTNESS |
Range: |
|
Describe: |
Returns the current internal reading from the on-board ambient light sensor. Note the optional keywords of RANGE and AVERAGE can be appended to the command to return the current RANGE setting for the BRIGHTNESS sensor if set or the current AVERAGE value applied when reading the ADC to obtain the reading. READ BRIGHTNESS |
Result: |
Read on-board light sensor level. |
Type or |
Control |
Command: |
BRIGHTNESS AVERAGE Advanced user
|
---|---|
Command Syntax: |
READ BRIGHTNESS.AVERAGE |
Range: |
|
Describe: |
Returns the current internal reading from the on-board ambient light sensor. Note the optional keywords of RANGE and AVERAGE can be appended to the command to return the current RANGE setting for the BRIGHTNESS sensor if set or the current AVERAGE value applied when reading the ADC to obtain the reading. READ BRIGHTNESS AVERAGE |
Result: |
Read on-board light sensor level. |
Type or |
Control |
Command: |
BRIGHTNESS RANGE Advanced user
|
---|---|
Command Syntax: |
READ BRIGHTNESS.RANGE |
Range: |
|
Describe: |
Returns the current internal reading from the on-board ambient light sensor. Note the optional keywords of RANGE and AVERAGE can be appended to the command to return the current RANGE setting for the BRIGHTNESS sensor if set or the current AVERAGE value applied when reading the ADC to obtain the reading. READ BRIGHTNESS RANGE |
Result: |
Read on-board light sensor level. |
Type or |
Control |