Command: |
ANALOG.IN i
|
---|---|
Command Syntax: |
READ.ANALOG.IN i |
Range: |
|
Describe: |
Generic analog input sensor. READ ANALOG.IN i – will return the ADC reading on the analog input associated with the object. |
Result: |
Reads generic ANALOG.IN input object |
Type or |
Sensor |
Command: |
ANALOG.IN i AVERAGE Advanced user |
---|---|
Command Syntax: |
READ.ANALOG.IN i AVERAGE |
Range: |
|
Describe: |
READ ANALOG IN i AVERAGE – gets the current averaging value for the object. |
Result: |
Reads generic ANALOG.IN input object |
Type or |
Sensor |
Command: |
ANALOG.IN i RANGE Advanced user |
---|---|
Command Syntax: |
READ.ANALOG.IN i RANGE |
Range: |
|
Describe: |
READ ANALOG IN i RANGE – returns the upper and lower range values associated with the object if specified, or error otherwise |
Result: |
Reads generic ANALOG.IN input object |
Type or |
Sensor |