The VERSION command has a response that represents the current version of the sketch running on the TI-Innovator™ Hub.
The version will be of the major.minor.patch.build form in released products; for example, 1.0.0.
Command: |
VERSION |
---|---|
Command Syntax: |
VERSION |
Describe: |
Returns version number (and possibly Accurev stream name from which sketch was built). |
Result: |
Report the version of the sketch in format major.minor.patch.build. Send ("VERSION") Get Str0 Disp Str0 |
Type or |
|