ISTI

The ISTI command is used to synchronize communications with the sketch. The response to this command must be TISTEM. Responses may have a leading NUL (0) character on initial power-on of the Innovator hub. All responses from the Innovator hub will be followed with a CR/LF pair that may or may not be stripped by software layers in the host system prior to the response being received by the application layer on the host system.

ISTI

Command:

ISTI

Command Syntax:

ISTI

Describe:

Send "ISTI", and get response "TISTEM".

Result:

Handshake command used to determine presence of a supported “sketch” on the TI-Innovaotr™ Hub.

Type or
Addressable Component: