POWER

Command:

CONNECT POWER n [TO] OUT1/OUT2/OUT3

Command Syntax:

CONNECT POWER n [TO] OUT1/OUT2/OUT3

Range

Describe:

Connects a POWER object to the specified analog output port.

Default PWM value is zero.

Result:

The named POWER device can be used in the program after a CONNECT command.

Type or
Addressable Component:

Control