Command: |
CONNECT RGB |
---|---|
Command Syntax: |
CONNECT RGB |
Range |
n/a |
Describe: |
This command configures the sketch to use the TI-RGB Array. The array needs to be pre-connected through the BB port. An incorrect connection will result in an error indication. |
Result: |
The RGB array is now available for use in the program. |
Type or |
Sensor |