Command: |
ANALOG.IN i [TO] IN n/BB n |
---|---|
Command Syntax: |
CONNECT ANALOG.IN i [TO] IN n/BB n |
Range: |
|
Describe: |
Connect a generic “analog” input sensor to a pin/port that supports analog input. CONNECT ANALOG.IN i [TO] IN 1 CONNECT ANALOG.IN i [TO] BB 5 |
Result: |
Connect analog input to pin that supports that function (error if pin is not analog-input capable). |
Type or |
Sensor |