You are here: TI-30X Pro MathPrint™ Scientific Calculator > Getting Started > Last Answer

Last Answer

% i

The last entry performed on the home screen is stored to the variable ans. This variable is retained in memory, even after the calculator is turned off. To recall the value of ans:

• Press % i (ans displays on the screen), or
• Press any operations key (T, U, and so forth) in most edit lines as the first part of an entry. ans and the operator are both displayed.

Examples

ans

3 V 3 <

 

V 3 <

 

3 % c % i <

Note: The variable ans is stored and pastes in full precision which is 13 digits.