G
|
|
---|---|
Keyword Description: Use global to create global variables inside a function. See CircuitPython documentation for more details. |
y N
|
|
|
---|---|
Module: ti_plotlib Syntax: plt.grid(xscl,yscl,"style") Description: Displays a grid using specified scale for x and y axes. Note: All plotting takes place when Setting grid color is the optional argument of (r,g,b) using values 0-255 with default value of gray (192,192,192). Default value for "style" = "dot" (default), "dash", "solid" or "point" Example: |
|
|
|
---|---|
Module: ti_plotlib Syntax: plt.grid(xscl,yscl,"style",(r,g,b)) Description: Displays a grid using specified scale for x and y axes. Note: All plotting takes place when Setting grid color is the optional argument of (r,g,b) using values 0-255 with default value of gray (192,192,192). Default value for "style" = "dot" (default), "dash", "solid" or "point" . If the xscl or yscl values are less than 1/50th of the difference between xmax-xmin or ymax-ymin, then an exception of 'Invalid grid scale value.' Example: See sample program: GRAPH. |
|