A
|
|
---|---|
Delimiter Syntax: Description: In Python, a comment begins with the hash tag character, #, and extends to the end of the line. Example:
|
y N
[a A #]
|
|
|
---|---|
Operator Syntax: Description: Returns remainder of Example:
See also |
y N
[a A #]
|
|
|
---|---|
Operator Syntax: Description: Returns the floor division of Example:
|
y N
[a A #]
|
|
|
---|---|
Description: Launch Includes accented characters such as ç à â è é ê ë î ï ô ö ù û |
|
|
|
---|---|
Module: ti_plotlib Syntax: plt.a gradient; slope Description: After Default values: = 0.0 Example: See sample program: LINREGR. |
|
|
|
---|---|
Module: Built-in Syntax:
Description: Returns the absolute value of a number. In this release, the argument may be an integer or floating point number. Example:
|
y N
Note: |
|
|
---|---|
Syntax: Description: Returns arc cosine of x in radians. Example:
Alternate Example: [Tools] > 6:New Shell
|
˜ 7:acos()
y N
[Fns…] Modul 1:math… > Trig
import commands can be found in |
|
|
---|---|
Keyword Syntax: Description: May return True or False. Returns Example:
|
y :
[Fns…] > Ops
y N
[a A #] |
|
|
---|---|
Module: Built-in Syntax: Description: The method Example:
|
y 9
y N
[Fns…] > List |
|
|
---|---|
Keyword Description: Use as to create an alias when importing a module. See Python documentation for more details. |
y N |
|
|
---|---|
Module: math Syntax:
Description: Returns arc sine of x in radians. Example:
Alternate Example:
|
˜ 6:asin()
y N
[Fns…] > Modul
import commands can be found in |
|
|
---|---|
Keyword Description: Use assert to test a condition in your code. Returns None or if not, execution of the program will display an AssertionError. |
y N |
|
|
---|---|
Module: math Syntax:
Description: Returns arc tangent of x in radians. Example:
Alternate Example:
|
˜ 8:atan()
[Fns…]>Modul 1:math... > Trig
y N
import commands can be found in |
|
|
---|---|
Module: math Syntax:
Description: Returns arc tangent of y/x in radians. Result is in Example:
Alternate Example:
|
˜ 9:atan2()
[Fns…] > Modul 1:math... > Trig
y N
import commands can be found in |
|
|
---|---|
Module: ti_plotlib Syntax: plt.auto_window(xlist,ylist) Description: Autoscales the plotting window to fit the data ranges within xlist and ylist specified in the program prior to the Note: max(list) - min(list) > 0.00001 Example: See sample program: LINREGR. |
|
|
|||||||||
---|---|---|---|---|---|---|---|---|---|
Module: ti_plotlib Syntax: plt.axes("mode") Description: Displays axes on specified window in the plotting area. Argument: "mode" argument options:
Example: See sample program LINREGR. |
|