Execution Error: Go to Program Line using Shell >Tools
The TI-Python experience will display Python error messages in the Shell when code is executed. If an error is displayed when a program executes, a program line number will display. Use Shell>Tools 7:Go to Program Line⦠Enter the line number and press [OK]. The cursor will display on the first character of the appropriate program line in the Editor. The program line number is displayed in the second line of the Status bar in the Editor.