rgb_array("lamp")

Command:

rgb_array("lamp")

Command
Syntax:

var = rgb_array("lamp")

Python
Code
Sample:

a1 = rgb_array("lamp")

Range:

N/A

Describe:

This command will enable the "high brightness" mode of the TI-RGB Array as long as an external power source (like the USB battery) is connected to the PWR port.

Note: "lamp" will need to be typed in.

Result:

The TI-RGB Array is now configured to be in high-brightness mode. If the external power is not connected, the "LAMP" has no effect

– i.e. the brightness will be at the default level. Also note, an error will be indicated by a beep tone.

Type or
Addressable
Component:

All components of the TI-RGB Array