Potentiometer
POTENTIOMETER is Generic variable resistance/potentiometer support interfaces.
Add Input Device
Item |
Description |
---|---|
Potentiometer |
Supports a potentiometer sensor. The range of the sensor can be changed by the range() function. |
CE products: from potentio import *
TI-Nspire CX II: from ti_hub import *
|
|
|
The function to create the object is pasted from the menu.
var=potentiometer("port")
Command: |
var=potentiometer("port") |
---|---|
Command |
var=potentiometer("port") |
Range: |
|
Describe: |
Creates an object for the potentiometer sensor. |
Result: |
|
Type or |
Control |
var.measurement()
Command: |
var.measurement() |
---|---|
Command |
var.measurement() |
Python |
TI Nspire CX II: from ti_hub import * p1 = potentiometer("IN 1") r = p1.measurement() print("Value is: ", m) |
|
CE products: from potentio import * p1 = potentiometer("IN 1") r = p1.measurement() print("Value is: ", r) |
Range: |
|
Describe: |
Returns the measured value of the potentiometer. |
Result: |
|
Type or |
Control |
var.range(min,max)
Command: |
var.range(min,max) |
---|---|
Command |
var.range(min,max) |
Range: |
|
Describe: |
Sets the range of returned values for the potentiometer. This needs to be called before the “var.measurement()” function for it to take effect. |
Result: |
|
Type or |
Control |