Moisture
MOISTURE is the soil moisture sensor support module.
Add Input Device
Item |
Description |
---|---|
Moisture |
Returns the moisture sensor reading. |
CE products: from moisture import *
TI-Nspire CX II: from ti_hub import *
|
|
|
The function to create the object is pasted from the menu.
var=moisture("port")
Command: |
var=moisture("port") |
---|---|
Command |
var=moisture("port") |
Range: |
|
Describe: |
Create an object for the moisture sensor attached to the “port”. |
Result: |
|
Type or |
Control |
var.measurement()
Command: |
var.measurement() |
---|---|
Command Syntax: |
var.measurement() |
Python |
TI Nspire CX II: from ti_hub import * m1 = moisture("IN 1") m = m1.measurement() print("Moisture is: ", m) |
|
CE products: from moisture import * m1 = moisture("IN 1") m = m1.measurement() print("Moisture is: ", m) |
Range: |
|
Describe: |
Returns the moisture value measured by the sensor. |
Result: |
|
Type or |
Control |
var.range(min,max)
Command: |
var.range(min,max) |
---|---|
Command |
var.range(min,max) |
Range: |
Default range: 0 - 16383 |
Describe: |
Sets the range of returned values for the sensor. This needs to be called before the “var.measurement()” function for it to take effect. |
Result: |
|
Type or |
Control |