Input
Input Devices
The Python interface to the sensors requires the creation of an object that represents the sensor. This includes specifying the port on the TI-Innovator™ Hub to which the sensor is attached.
The sensor readings can then be read through the ".measurement()" function for each sensor.
Here are the input devices and their associated functions.