LightLevel (Light Sensor)
LIGHTLEVEL supports reading external light level sensors.
Add Input Device
Item |
Description |
---|---|
Light Level |
Returns the brightness level from the external light level (brightness) sensor. |
CE products: from lightlvl import *
TI-Nspire CX II: from ti_hub import *
|
|
|
The function to create the object is pasted from the menu.
var=light_level("port")
Command: |
var=light_level("port") |
---|---|
Command |
var=light_level("port") |
Range: |
|
Describe: |
Create an object for the light level sensor attached to the “port”. |
Result: |
|
Type or |
Control |
var.measurement()
Command: |
var.measurement() |
---|---|
Command Syntax: |
var.measurement() |
Python |
TI Nspire CX II: from ti_hub import * l1 = light_level("IN 1") b = l1.measurement() print("Light level is: ", b) |
|
CE products: from lightlvl import * l1 = light_level("IN 1") b = l1.measurement() print("Light level is: ", b) |
Range: |
|
Describe: |
Returns the relative brightness between 0 and 100 measured by the sensor. |
Result: |
|
Type or |
Control |
var.range(min,max)
Command: |
var.range(min,max) |
---|---|
Command |
var.range(min,max) |
Range: |
|
Describe: |
Sets the range of returned values for the sensor. This needs to be called before the “var.measurement()” function for it to take effect. |
Result: |
|
Type or |
Control |