Analog In
This object can be used to interface with analog sensors that are not explicitly supported
ANALOG.IN supports the use of analog input generic devices.
Add Input Device
Item |
Description |
---|---|
Analog In |
Supports the use of analog input generic devices. |
CE products: from analogin import *
TI-Nspire CX II:from ti_hub import *
|
|
|
The function to create the object is pasted from the menu.
var=analog_in("port")
Command: |
var=analog_in("port") |
---|---|
Command |
var=analog_in("port") |
Range: |
|
Describe: |
Creates an object for the analog input sensor attached to the “port” |
Result: |
|
Type or |
Control |
var.measurement()
Command: |
var.measurement() |
---|---|
Command |
var.measurement() |
Python |
TI Nspire CX II: from ti_hub import * an1 = analog_in("BB 5") val = an1.measurement() print("Analog In value: ", val) |
|
CE products: from analogin import * an1 = analog_in("BB 5") val = an1.measurement() print("Analog In value: ", val) |
Range: |
|
Describe: |
Returns the sensor data value. Default range is 0 – 16383. |
Result: |
|
Type or |
Control |
var.range(min,max)
Command: |
var.range(min,max) |
---|---|
Command |
var.range(min,max) |
Range: |
|
Describe: |
Sets the range of returned values for the sensor. This needs to be called before the “var.measurement()” function for it to take effect. |
Result: |
|
Type or |
Control |