RV.COLORINPUT
Command: |
RV.COLORINPUT |
||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Command Syntax: |
RV.COLORINPUT |
||||||||||||||||||||
Code |
Send("READ RV.COLORINPUT") Get(C) |
||||||||||||||||||||
Range: |
1 thru 9 |
||||||||||||||||||||
Describe: |
Bottom-mounted color sensor detects the color of the surface. Can also detect gray-level scale of black (0) to white (255).
|
||||||||||||||||||||
Result: |
Returns current color sensor information. The return value is in the 1 – 9 range which maps to the colors below:
|
||||||||||||||||||||
Type or |
Sensor Note: This Rover sensor command is executed immediately. |