Preparing TI-Innovator™ Rover

Follow these steps to fully charge your TI-Innovator™ Rover.

1. Identify the Micro connector on the USB Standard A to Micro cable.

2. Insert the Micro connector into the PWR port on the side of the Rover.

3. Insert the free end of the cable (the "A" connector) into the USB port on your computer or TI Wall Charger.

 

Note: The Battery Level Indicator shows solid green when the battery is fully charged.

Make sure the TI-Innovator™ Rover is switched OFF before connecting to the
TI-Innovator™ Hub.

▶ Flip the On/Off (I/O) switch to the Off (O) position.