Drive RV...

RV Drive Command Families

• Base Drive Commands (in the spirit of Turtle Graphics)
- FORWARD, BACKWARD, RIGHT, LEFT, STOP, STAY
• Math Coordinate Drive Commands
- Turn to Angle

Note: Drive commands have options for Speed, Time and Distance as appropriate

• See RV Settings for Machine-Level Control Commands
- Set Left and Right Motor values for direction (CW/CCW) and level (0-255,Coast)
- Read accumulated values for wheel encoder edges and gyro heading change.

Commands for Drive RV...

CE Calculators

TI‑Nspire™ CX