TI-RGB Array Commands Version 1.5
Prerequisite: Use the Send "Connect RGB" Command First
The "CONNECT RGB" command needs to be used first when using the TI-RGB Array. The "CONNECT RGB" command configures the TI-Innovator™ Hub software to work with the TI-RGB Array.
It establishes the connections to the various led binary slots on the TI-RGB Array – 0 through 15 RGB LED. It also clears the various counters and sensor values.