THERMISTOR i
|
Command: |
THERMISTOR i
|
|---|---|
|
Command Syntax: |
READ THERMISTOR i |
|
Range: |
|
|
Describe: |
Returns the current temperature reading from the associated thermistor sensor. Temperature is returned in Celsius. |
|
Result: |
Return current thermistor temperature in Celsius. |
|
Type or |
Sensor |
THERMISTOR i AVERAGE
|
Command: |
THERMISTOR i AVERAGE Advanced user
|
|---|---|
|
Command Syntax: |
READ THERMISTOR i AVERAGE |
|
Range: |
|
|
Describe: |
Returns the current temperature reading from the associated thermistor sensor. Temperature is returned in Celsius. |
|
Result: |
Return current thermistor temperature in Celsius. |
|
Type or |
Sensor |
THERMISTOR i CALIBRATION
|
Command: |
THERMISTOR i CALIBRATION
Advanced user
|
|---|---|
|
Command Syntax: |
READ THERMISTOR i CALIBRATION |
|
Range: |
|
|
Describe: |
Returns the current temperature reading from the associated thermistor sensor. Temperature is returned in Celsius. |
|
Result: |
Returns list with current {c1,c2,c3,r} values used for connected thermistor. |
|
Type or |
Sensor |