Command:
RESOLUTION
Command Syntax:
READ RESOLUTION
Range:
Describe:
Returns the bit resolution used by the system for ADC readings.
Result:
Returns ADC resolution in use, in bits (default is 14).
Type or Addressable Component:
Setting