POTENTIOMETER i
|
Command: |
POTENTIOMETER i
|
|---|---|
|
Command Syntax: |
READ POTENTIOMETER i |
|
Range: |
|
|
Describe: |
Read analog value of the potentiometer (linear or rotary). The optional AVERAGE and RANGE keywords can be appended to the command to obtain the current average count, or mapped range being used, if present, for the given potentiometer. READ POTENTIOMETER i READ POTENTIOMETER i RANGE READ POTENTIOMETER i AVERAGE |
|
Result: |
Read analog value of rotary encoder / potentiometer (uses averaging). |
|
Type or |
Sensor |
POTENTIOMETER i AVERAGE
|
Command: |
POTENTIOMETER i AVERAGE Advanced user
|
|---|---|
|
Command Syntax: |
READ POTENTIOMETER i AVERAGE |
|
Range: |
|
|
Describe: |
Read analog value of the potentiometer (linear or rotary). The optional AVERAGE and RANGE keywords can be appended to the command to obtain the current average count, or mapped range being used, if present, for the given potentiometer. READ POTENTIOMETER i AVERAGE |
|
Result: |
Read analog value of rotary encoder / potentiometer (uses averaging). |
|
Type or |
Sensor |
POTENTIOMETER i RANGE
|
Command: |
POTENTIOMETER i RANGE Advanced user
|
|---|---|
|
Command Syntax: |
READ POTENTIOMETER i RANGE |
|
Range: |
|
|
Describe: |
Read analog value of the potentiometer (linear or rotary). The optional AVERAGE and RANGE keywords can be appended to the command to obtain the current average count, or mapped range being used, if present, for the given potentiometer. READ POTENTIOMETER i RANGE |
|
Result: |
Read analog value of rotary encoder / potentiometer (uses averaging). |
|
Type or |
Sensor |