LED i
|
Command: |
LED i
|
|---|---|
|
Command Syntax: |
READ LED i |
|
Range: |
|
|
Describe: |
Read the current state of the specified LED. If the LED is digital, a 0 or 1 is returned indicating the LED is off or on. If the LED is connected to a PWM output, a value from 0 to 255 will be returned, indicating the current PWM level where 0 is off, 255 is full on, and values in between indicate the current PWM setting. |
|
Result: |
Get state of LED, 0 or 1 if digital, 0-255 if PWM on analog. |
|
Type or |
Control |