ANALOG.IN i
|
Command: |
ANALOG.IN i
|
|---|---|
|
Command Syntax: |
READ.ANALOG.IN i |
|
Range: |
|
|
Describe: |
Generic analog input sensor. READ ANALOG.IN i – will return the ADC reading on the analog input associated with the object. |
|
Result: |
Reads generic ANALOG.IN input object |
|
Type or |
Sensor |
ANALOG.IN i AVERAGE
|
Command: |
ANALOG.IN i AVERAGE Advanced user |
|---|---|
|
Command Syntax: |
READ.ANALOG.IN i AVERAGE |
|
Range: |
|
|
Describe: |
READ ANALOG IN i AVERAGE – gets the current averaging value for the object. |
|
Result: |
Reads generic ANALOG.IN input object |
|
Type or |
Sensor |
ANALOG.IN i RANGE
|
Command: |
ANALOG.IN i RANGE Advanced user |
|---|---|
|
Command Syntax: |
READ.ANALOG.IN i RANGE |
|
Range: |
|
|
Describe: |
READ ANALOG IN i RANGE – returns the upper and lower range values associated with the object if specified, or error otherwise |
|
Result: |
Reads generic ANALOG.IN input object |
|
Type or |
Sensor |