ISTI
The ISTI command is used to synchronize communications with the sketch. The response to this command must be TISTEM. Responses may have a leading NUL (0) character on initial power-on of the Innovator hub. All responses from the Innovator hub will be followed with a CR/LF pair that may or may not be stripped by software layers in the host system prior to the response being received by the application layer on the host system.
ISTI
|
Command: |
ISTI |
|---|---|
|
Command Syntax: |
ISTI |
|
Describe: |
Send "ISTI", and get response "TISTEM". |
|
Result: |
Handshake command used to determine presence of a supported “sketch” on the TI-Innovaotr™ Hub. |
|
Type or |
|