eval(
|
Command: |
eval( |
|---|---|
|
Command Syntax: |
eval(Expr) ⇒string |
|
Range |
|
|
Describe: |
The software evaluates expression Expr and replaces the eval() statement with the result as a character string. The argument Expr must simplify to a real number.
CE Calculators: eval() can be used as a standalone command outside a TI-Innovator™ Hub command. TI-Nspire™ CX platform: eval() is valid only in the TI-Innovator™ Hub Command argument of programming commands Get, GetStr, and Send. |
|
Result: |
CE Calculators: For debugging purposes, using the command line Disp Ans immediately after a command line using Send( displays the complete string being sent. TI-Nspire™ CX platform: Although eval() does not display its result, you can view the resulting Hub command string after executing the command by inspecting any of the following special variables. iostr.SendAns iostr.GetAns iostr.GetStrAns |
|
Type or |
Not Applicable |