MAGNETIC
|
Command: |
DISCONNECT MAGNETIC i |
|---|---|
|
Command Syntax: |
DISCONNECT MAGNETIC 1 |
|
Range |
|
|
Describe: |
The MAGNETIC sensor is used to detect the presence of a magnetic field. It uses the Hall effect. It is also known as a Hall effect sensor.
The DISCONNECT command removes the sensor from the program. |
|
Result: |
The name “MAGNETIC 1” is now disconnected from the sensor. It cannot be used in the program after a DISCONNECT command. |
|
Type or |
Sensor |